Perform Nonvolatile Memory Operations

The
Nonvolatile Memory
tab of the
Controller Properties
dialog box serves as the starting point from which you can perform nonvolatile memory operations. Click the
Load/Store
button to access the
Nonvolatile Memory Load/Store
dialog box, from which you can perform the actual operations.
The Nonvolatile Memory tab also provides you with status information that indicates any conditions that might prevent you from loading or storing. Possible status messages include:
  • Nonvolatile memory not present
  • Nonvolatile memory not available in the current module redundancy state
  • Controller being edited by another user
  • No controller image or stored controller image
  • Controller not in Program mode
  • Stored image revision in nonvolatile memory does not match controller revision
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.