Import Configuration dialog box - Configure Equipment Sequence properties
Use this dialog box to configure how the
Equipment Sequence
is imported into the project. When you select the Equipment Sequence
or one of its parts in the Import Content
pane, the configuration properties associated with that part of the Equipment Sequence
are displayed in the Details pane.
TIP:
To open the Import Configuration dialog box - Configure Equipment Sequence properties dialog:
- SelectFile > Import Component > Equipment Sequence.
- Select a sequence for import and selectOpen.
Use the dialog box to:
- Configure basic properties for the importedEquipment Sequence, such as the name for the sequence when it is imported into the project, and which task you want to put it in.
- View and adjust the imported sequence's configuration properties that match or conflict with existing settings in your project. To see the configuration properties, click the items in theImport Contentpane, such asParameters and Local Tag definitions,Routines, andTags.
- View messages, such as errors and warnings, related to the import.
Provide Feedback