Function Block Properties Dialog Box - SBR Properties

The Subroutine (SBR) instruction receives the input parameters passed by the JSR and perform the functions in the logic.
Use the
SBR Properties
tab of the
Function Block Properties
dialog box to set the values for the parameters of the selected SBR instruction.
The following table describes the parameter attributes available on the
SBR Properties
tab:
Attributes
Description
Parameters
Enter a tag name to be used for the parameter. You can enter a tag name by typing it directly into the box, or by choosing an available tag from the tag browser, which appears when you click the pull-down menu.
You must start a pending edit to modify the routine name.
OK
Click this button to add the selected item in the instruction list to the routine and close the
Function Block Properties
dialog box.
If you are online, the changes are sent to the controller when you accept the pending edit.
Cancel
Click this button to cancel any edits you have made and close the
Function Block Properties
dialog box.
Apply
Click this button to accept your changes and continue editing in the
Function Block Properties
dialog box.
If you are online, the changes are sent to the controller when you accept the pending edit.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.