Enable and disable project Automatic Diagnostics
Automatic Diagnostics automatically sends device diagnostic condition updates to applications and client devices supported by
FactoryTalk Alarms and Events
. Automatic Diagnostics is enabled by default.
TIP:
Automatic Diagnostics is supported only on
CompactLogix
5380, CompactLogix
5480, ControlLogix
5580, Compact GuardLogix
5380, and GuardLogix
5580 controllers.To Enable or disable Automatic Diagnostics:
- On the main menu, selectEdit > Controller Properties.
- Select theAdvancedtab.
- Select or clear theEnable Automatic Diagnosticscheck box.
Provide Feedback