Edit Action properties

Edit Action properties to change the type, preset, timer, and other properties of the action.
To edit action properties:
  1. From
    Qualifier
    , select the qualifier to determine when an action is executed.
    The "N" qualifier, for example, causes an action to execute as long as its associated step is active. As another example, the P1 qualifier causes an action to execute only once when its associated step is first activated. For more information, see
    Action Properties - General
    .
    Choose from:
    • N - Non-stored
    • R - Reset
    • S - Stored
    • L - Time Limited
    • D - Time Delayed
    • P - Pulse
    • P1 - Pulse (Rising Edge)
    • P0 - Pulse (Falling Edge)
    • SL - Stored and Time Limited
    • SD - Stored and Time Delayed
    • DS - Time Delayed and Stored
  2. Select
    Boolean
    if this action is a Boolean action.
  3. In
    Preset
    , enter a value for the PRE action tag member.
    Configure Preset as a DINT value or as the result of an expression. To use an expression, select
    Use Expression
    , then select
    Define
    .
  4. In
    Timer
    , enter the T value of the action.
    This value indicates how long (in milliseconds) the Action was active during this activation. When an Action is first activated, this value is reset to 0. When an action is no longer active, this field retains the elapsed time, thereby reflecting how long the Action was active the last time it was activated.
  5. In
    Count
    , enter the Count value of the action.
    This value indicates how many times the Action was activated since the action Count was last reset. If this counter reaches its upper limit, the counter rolls over to 0 and continues counting. The Count is automatically reset when the SFC is reset.
  6. Select
    Pause Timer When Routine is Paused
    if the Action Timer should not increment while the SFC routine is paused. Clear the box to have the Action Timer jump forward when the SFC routine resumes execution after being paused. The Action Timer jumps forward by the amount of time of the pause.
  7. In
    Indicator Tag
    , enter an operand to appear in the action display in the sequential function chart routine.
    Select
    New Tag
    to create a new tag for this option.
  8. Select
    OK
    to apply the edits and close
    Action Properties
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.