Edit Transition properties

Edit Transition properties

Edit Transition properties to change the settings for a transition.
To edit transition properties
  1. Select
    Never Display Description in Routine
    to never display the transition’s description within the sequential function chart routine, even if the option on the
    Workstation Options
    dialog box is set to show descriptions.
    This check box applies to the current transition only; if the Workstation Options item is set to show descriptions, they are shown for all other transitions (unless description display is turned off for them individually).
  2. Select
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal