Layout Selected SFC Elements command

Choose this command to:
  • Remove unnecessary slack between connected SFC elements (i.e., shorten wires), where possible
  • Justify branches
  • Move unconnected elements during the layout process, to maintain relative position to other elements that might have moved
  • Move elements that are too close to the left of the diagram or are on a page boundary
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.