You can use this workstation to manually configure safety relays and input devices in a relay-based safety system. You can actuate the input devices to see how the safety relays monitor and control machine systems. Using the single wire safety feature between relays you can configure interdependent devices and zoning options.
The workstation includes switches that are hard-wired to simulate wiring and device faults for use in troubleshooting the safety system. The workstation offers expansion capabilities by providing a connection for a safety drive’s STO inputs (drive and custom cable not included).