Pre-engineered, prepackaged safety instrumented system designed for applications up to 100 I/O points
MILWAUKEE, May 4, 2015 — Rockwell Automation has introduced its new OptiSIS solution, giving industrial operators a pre-engineered safety instrumented system that can help ease deployment and reduce lead times for small and midsized process applications.
The OptiSIS solution is ideal for oil and gas, chemical and petrochemical producers with aging process-safety systems that are either noncompliant or can no longer be maintained.
“Replacing or upgrading a process-safety system using a custom-engineered approach can be costly and time-consuming,” said Mark Eldredge, Packaged Solutions program manager for Rockwell Automation. “The OptiSIS solution can reduce lead time by more than 30 percent, leading to faster and more cost-effective safety instrumented system deployments.”
The OptiSIS solution is designed for safety instrumented system applications of 50 or 100 I/O points, including emergency shutdown (ESD) systems, burner-management systems (BMS) and high-integrity pressure protection systems (HIPPS). The version for applications of up to 100 I/O points will be available in the fourth quarter of 2015.
“Packaged solutions from Rockwell Automation are designed to help industrial operators fill capability gaps and address their specific business challenges,” said Allan Rentcome, global technology director for Systems and Solutions at Rockwell Automation. “With the OptiSIS solution, industrial operators now have a packaged solution for safety applications that historically may have been too small to justify the investment.”
The pre-engineered OptiSIS solution is delivered ready to install, wire and configure, shortening the overall engineering time and eliminating the need for any programming. Users need only enter their logic scenarios into the system’s cause-and-effect graphical interface. The configurations are tested and can then be stored for verification against original safety function requirements – or used at a later date to restore the system to a known state.
Flexible inputs and outputs help confirm that the system accommodates a varying mix of digital and analog I/O types. Additionally, simplex I/O and fault-tolerant (dual) I/O versions are available to address different redundancy needs.
The system meets requirements up to Safety Integrity Level 3 (SIL 3) and is compliant with IEC 61511/ISA 84.00.01. It uses ready-to-install, TUV-certified hardware and validated application software.
Rockwell Automation will demonstrate the new OptiSIS solution at the Offshore Technology Conference (OTC) in Booth 11813, taking place May 4 to 7 in Houston.
News Release Assets
Image available upon request or here at box.com.
About Rockwell Automation
Rockwell Automation Inc. (NYSE: ROK), the world’s largest company dedicated to industrial automation and information, makes its customers more productive and the world more sustainable. Headquartered in Milwaukee, Wis., Rockwell Automation employs about 22,500 people serving customers in more than 80 countries.
Media Contacts
Marilyn Muscenti
Rockwell Automation
440.646.4087
memuscenti@ra.rockwell.com
Molly O’Mara
PadillaCRT
612.455.1918
molly.omara@padillacrt.com
LISTEN. THINK. SOLVE. and OptiSIS are trademarks of Rockwell Automation Inc.
Published May 3, 2015