Controller-embedded MPC can help drive improvements in quality, throughput, yield and energy efficiency
MILWAUKEE, Nov. 2, 2015 — Rockwell Automation will release PlantPAx model predictive control (MPC) software, which for the first time embeds fully functional MPC technology into Logix controllers to help maximize equipment performance. When used in process applications ranging from consumer to heavy industries, PlantPAx MPC can improve overall control in a single machine or an entire line to help maximize throughput, increase yield, reduce quality variability and improve energy usage.
PlantPAx MPC is included in the latest release of the PlantPAx modern distributed control system.
“By embedding MPC into the control system, PlantPAx MPC simplifies integration and improves ease of use,” said Mike Tay, product manager, Rockwell Automation. “It also delivers several performance advantages over single-loop PID controllers. These include better multivariable coordination, predictable handling of outside disturbances, improved management of long or complex processes and predictive response to process constraints, all resulting in maximizing equipment performance while safely operating within process limits.”
Multivariable Coordination: PlantPAx MPC delivers better coordination of multivariable actions in complex process applications to maximize controller performance and maintain quality. A single control-system-based MPC module supports up to five separate MPC applications, and each of those applications can support up to 10 controllable variables and 10 manipulated variables.
Predictably Handle Outside Disturbances: The software provides the ability to measure disturbance variables that can’t be controlled, such as ambient humidity. Once detected, the system can predictably respond to these disturbances as needed to keep the process optimized.
Manage Long and Complex Processes: Both operators and control systems can struggle when managing long and complex processes for applications, such as dryers and kilns. PlantPAx MPC uses dynamic explicit modeling to identify and program the specific responses and requirements for these processes.
Predictive Response to Constraints: PlantPAx MPC dynamically predicts process behavior against identified constraints and makes proactive adjustments to maintain process performance within identified limits.
Maximize Equipment Performance: Dynamic and steady-state constraints can be enforced in the software to maximize equipment performance up to its limits. For example, enforcing a flooding constraint in a distillation process can help feed levels at their highest without the risk of flooding.
PlantPAx MPC will be on display at the Process Solutions Booth 1078 during the 2015 Automation Fair event from Rockwell Automation, taking place Nov. 16 to 19 at McCormick Place West in Chicago. It will also be featured in the session “Applications for PlantPAx MPC” at the Process Solutions User Group (PSUG) during the Automation Fair event.
News Release Assets
Image available upon request or here at box.com.
About Rockwell Automation
Rockwell Automation Inc. (NYSE: ROK), the world’s largest company dedicated to industrial automation and information, makes its customers more productive and the world more sustainable. Headquartered in Milwaukee, Wis., Rockwell Automation employs about 22,500 people serving customers in more than 80 countries.
Media Contacts
Mike Orona
Rockwell Automation
512.438.1482
mlorona@ra.rockwell.com
Molly O’Mara
PadillaCRT
612.455.1918
molly.omara@padillacrt.com
Automation Fair, LISTEN. THINK. SOLVE. and PlantPAx are trademarks of Rockwell Automation Inc.
Published November 1, 2015