Asset Intelligence Features

Asset Intelligence Features

Features List
S.No
Features
Description
1
Asset Intelligence Dashboards
It helps the user to visualize the KPI health, get the top underperforming asset at all levels, and access the triggered alerts at each node.
2
Asset Setup
It helps the user to create an asset hierarchy structure, configure sensors and KPIs at the asset and component level.
3
Function Setup
It helps the user to create custom equations and view the available KPI and ML functions.
4
Notification Setup
It helps the user to configure notification for an asset or asset group.
5
Dashboard Setup
It helps the user to configure default KPIs to be displayed on the cards throughout the application.
6
Asset Model Setup
It helps the user to preview, import, and export asset model templates.
7
User Management
It helps the user to create roles, manage user access and resources such as asset class and Sites.
8
Modifying the Hierarchy
It helps the user to modify the hierarchy structure by moving the hierarchy node.
9
Favorites
It helps the user to have a list of nodes added to favorites for easy access or navigation.
10
Compare
It helps the user to compare assets within an asset class and analyze their common and uncommon KPI Health and their component's risk score.
11
Underperforming Assets
It helps the user to analyze the top 5,10,20,100 underperforming assets across any level in the hierarchy considering their common KPIs.
12
Trending
It helps the user to visualize the Sensors or KPI's health and get useful insights from their data.
13
Alerts
It helps the user to visualize the Sensors or KPI's health and get useful insights from their data.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal