Conventions

Conventions

The following conventions are followed in this document:
  • Text, labels, and icon names that are in the User Interface appear in square brackets. For example: Click [Manage Profile].
  • Placeholder text for variable values appears in angle brackets. For example:
    https://<FQDN-hostname>/<install folder>
  • The URLs and links appear in blue text. For example: Application Link.
  • The Cross-Reference appears in blue text. For example: Getting Started.
  • The information requiring special attention is in bold text.
    For example:
    IMPORTANT:
    Use a complex password as per the company policy.
  • The toast messages that are displayed on the User Interface appear in the italic text and the quotation. For example: The "
    NA was added under the Enterprise successfully
    ” message displays.
    Toast Messages
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal