Remove favorites

Remove Favorites

You can remove favorites from any cards at any level from the favorites section. Steps to remove favorites are similar for all levels of cards.
Perform the following steps to remove favorites from the Region card from the
Favorites
section:
  1. Select the [] icon from the left pane.
    Now you can see all types of favorite added cards.
  2. Click the [] expansion icon to view the cards.
  3. Click the [] icon on the respective card and select
    Remove Favorites
    .
    Select remove favorites
    Now the selected product is removed from the favorites section and the favorites icon [] is removed from the selected card. The "
    Card removed from favorites successfully
    ” message displays.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal