Asset Classes

Asset Classes

In the Asset Classes tab, you can view the list of available asset classes with status and association details in the table. Perform the following steps to add a new asset class:
  1. Click
    Configuration
    >
    Asset model setup
    from the menu bar.
  2. Select the
    Asset Classes
    tab and click [Add].
    Asset classes
  3. In the
    Add Asset Class
    window, set these parameters:
    • Asset Class Name
      : Select the asset class name from the drop-down list.
    • Asset Class Status
      : Select the asset class status from the drop-down list.
    • Asset Class Description
      : Provide the description of the asset class.
  4. Click [Add].
    Add Asset Class
    The “
    Asset Class added successfully
    ” message displays.
Perform the following steps to edit the asset class:
  1. Select the required asset class check box and click [Edit].
    NOTE: You can edit the asset class only if the asset class status is in draft or active with no association.
  2. Edit the fields and click [Save].
    The “
    Asset class updated successfully
    ” message displays.
Perform the following steps to delete the asset class:
  1. Select the required asset class check box and click [Delete].
    NOTE: You can delete the asset class only if the asset class status is in the draft status.
    The “
    Asset Class deleted successfully
    ” message displays.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.