Import Asset Model

Import Asset Model

Perform the following steps to import the asset model:
  1. Click
    Configuration
    >
    Asset model setup
    from the menu bar.
  2. Click [Import Asset Model].
    Import Asset Model
  3. In the
    Import Asset Model
    window, under
    Choose Asset Model
    tab, click
    Browse
    .
  4. Select the required file and Click [Import Asset Model].
    Preview Asset Model
The asset model is added to the
Asset Models
table.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.