Hierarchy Configuration

Hierarchy Configuration

Perform the following steps to configure KPI:
  1. Click
    Configuration
    >
    Dashboard setup
    from the menu bar.
  2. Click the
    Hierarchy Config
    tab and the Hierarchy Config page displays.
  3. In the
    Hierarchy Config
    tab, select the Tag Name and the Unit of Measurement from the drop-down lists.
  4. Select
    Enable KPI
    toggle button to view the throughput value in the cards.
  5. Click [Save].
    Hierarchy Configuration
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.