Configure Equation

Configure Equation

Perform the following steps to configure the equation:
  1. Click
    Configuration
    >
    Function setup
    from the menu bar.
  2. In the
    Equations
    tab, click [Create Equation].
    Basic Details
  3. In the
    Basic Details
    tab, set these parameters:
    • Equation Name
      : Provide the equation name.
    • Equation Description
      : Provide the description for the equation.
    • Version
      : Provide the version details
    • Equation Status
      : Select the status from the drop-down list.
  4. Click [Next].
    Basic Details
  5. In the
    Enter the Equation below
    box, provide the equation.
  6. Click [Validate].
    Validate Equation
    Guidelines for creating equation
  7. In the pop-up dialog, you can view the equation in the book format. Click [Confirm].
    Confirm Equation
  8. After the validation is successful, you will get the variable details in the Input and Output variable table.
    NOTE: If the validation is not successful, variable details will not be populated in the Input and Output variable table.
  9. Click [Next].
    Input variable details
  10. In the
    Equation Validation
    tab, perform the following actions:
    • Click [Test Function].
    • You will get the output value in the
      Output Generated
      box.
    • Click [Save].
      Test output
      The "
      Equation is added successfully
      " message displays. The equation is added to the table.
      Equation Details
Perform the following steps to edit the equation:
  1. Select the required equation check box from the table.
  2. Click [Edit] and edit the required fields.
  3. Click [Save].
Perform the following steps to delete the equation:
  1. Select the required equation check box from the table.
  2. Click [Delete].
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.