Active Alerts

Active Alerts

You can view the alerts related to all the nodes. There are two types of alerts such as active and historical alerts. Perform the following steps to view the active alerts:
  1. Click the [] icon from the menu bar.
  2. Select the required node from the hierarchy list in the left pane.
    In the
    Active Alerts
    tab, you can view all the alerts such as advisory, sensor fault, and KPI alerts. You can also view the overall and respective alert count of advisory, sensor fault, and KPI alerts.
    Active Alerts
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.