Add Favorites

Add Favorites

You can add favorites to any cards at any level. The steps to add favorites are similar for all levels of cards.
Perform the following steps to add favorites to the
Product
card:
  1. Select the required
    Region
    from the hierarchy list.
  2. Click the [] icon in the required card and select
    Add to favorites.
    Select Add to favorites
    The "
    Card added to Favorites successfully
    " message displays. Now the favorites icon [] is added to the selected card.
    Favorites icon
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.