Available Activations table

Available Activations table

The
Available Activations
table contains this information.
TIP:
Activations that are not available for use because of a disconnected Ethernet card or dongle may still appear in
Available Activations
.
TIP:
Node-locked activations and local-only activations on a remote or server computer do not appear in the list of available activations on a client computer. To make these activation types available on a client computer, rehost the node-locked or local-only activations on the server computer and either replace them with concurrent versions or download node-locked or local-only activations to the client computer.
Available Activations
does not indicate if a node-locked activation is not available for use because of a disconnected Ethernet card or dongle.
TIP:
Expired Flexera activations on remote computers that are listed in
Path to Activations
do not appear.
Name
Description
Product
The
Rockwell Automation
product.
Serial#
The serial number of the product.
Expires
The activation's expiration date.
Support Expires
The product support end date.
Activation
The name of the activation.
Feature Version
The feature version of the license.
Location
The name of the local or remote computer on which activations are downloaded for the product. For example,
Local: Borrowed
identifies an activation borrowed from an activation server and available on the local computer until the activation is returned or expires.
Total
The number of activations purchased with the product.
For concurrent activations,
n/a
displays if:
  • the activation is not available for use because of a disconnected Ethernet card or dongle.
  • the dongle hardware version and the dongle driver version do not match. Removing the existing dongle driver and then reinserting the dongle may install the correct driver and resolve this issue.
If you have both node-locked and concurrent activations for a product, the total number of concurrent activations aggregates the node-locked activation into its count and may display an unexpected value. You can still check out and use the activations.
In Use
The number of activations used for each product. Click the number in this column to see more details, such as the computer that checked out or borrowed the activation, the number of activations checked out or borrowed, and whether the activation is concurrent or borrowed. No details are available if the number in this column is zero.
Borrowed
The number of activations borrowed from an activation server. Click the number in this column to see more details, such as the computer that borrowed the activation, the date the activation was borrowed, and the date the borrowed activation expires. No details are available if the number in this column is zero.
Product Version
The product version activated. n/a if not used. Some activations are for multiple product versions. This field displays
n/a
if not used.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal