Execute Database Script

Execute Database Script

  1. Open the pgAdmin application. Double-click [Servers] and then double-click [PostgreSQL 13]. Provide the password to open pgAdmin.
  2. Right-click the FTADataView database and select the [Query Tool] option.
    Query Tool
  3. Maximize the pgAdmin4 window.
  4. Click the Folder icon on the tool bar.
    Folder
  5. Switch the Format field to “All Files” and go to the
    DataView
    install folder.
    Select File Format
  6. In the Select File dialog open the
    dbscripts
    folder in the
    <4.00.01_DataView_HOME>\FTADataView\dbscripts
    directory.
    IMPORTANT:
    If the files are extracted to a different folder other than the folder shown below, the folder/path instructions may be different.
    DB Script Folder
  7. Open the
    migrationscript
      folder.
  8. Select the
    4.00.00_To_4.00.01_DataViewScript.sql
    file and click [Select].
    Select Database Script
  9. The script is displayed under FTADataView database. Click the [ ] icon to execute the ‘4.00.00_To_4.00.01_DataViewScript.sql’.
    Run the 4.00.00to4.00.01.sql
  10. Refresh the database.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.