Prerequisites

Prerequisites

  • Power BI Desktop application is installed.
  • Access to FactoryTalk DataMosaix.
  • The Data Scientist role is assigned to create applications in FactoryTalk DataMosaix.
  • Register the application using the Machine-to-Machine type in FactoryTalk DataMosaix. For information on registering an application in FactoryTalk DataMosaix, refer to Register Application.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal