Datasource Connection using Tableau Cloud

Datasource Connection using Tableau Cloud

Perform the following steps to connect to data source using Tableau Cloud:
  1. In the browser, use your Site URL and press
    Enter
    .
  2. In the
    Tableau
    page, provide the username and password shared by the Tableau Admin and click
    Sign In
    .
    Tableau Sign in Page
  3. To create a new workbook, navigate to
    New
    >
    Workbook
    .
    Create New Workbook
  4. In the
    Connect to Data
    dialog box, click
    Connectors
    >
    PostgreSQL
    .
    Select PostgreSQL
    The
    PostgreSQL
    dialog box is displayed.
  5. Provide the following details:
    • Server:
      dm-virtualpostgres.cloud.rockwellautomation.com
      (Production URL).
    • Port: Provide port number as 5432.
    • Database: The name of the project in FactoryTalk DataMosaix.
    • Authentication: By default, Username and Password is selected.
    • Username: Refer to the Client ID generated while registering the application.
    • Password: Refer to the Client Secret generated while registering the application.
      NOTE:
      SSL is always enabled in both checked and unchecked conditions of the
      Require SSL
      checkbox.
  6. Click
    Sign In
    .
    PostgreSQL Dialog
  7. Drag and drop a table to open campus and click
    Update Now
    to get the table data.
    View Table Data
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal