Datasource Connection using Tableau Desktop

Datasource Connection using Tableau Desktop

Perform the following steps to connect to data source using Tableau Desktop:
  1. Open
    Tableau Desktop
    .
  2. Click
    Activate by signing in to a server
    .
    Activate Tableau
    The
    Tableau Server Sign In
    dialog box is displayed.
  3. Click
    Connect
    .
    Tableau Server Sign In Dialog
  4. Provide the username and password shared by the Tableau Admin and click
    Sign In
    .
    Sign In Page
  5. Navigate to
    Connect
    >
    To a server
    >
    More…
    >
    PostgreSQL
    .
    Select PostgreSQL
    The
    PostgreSQL
    dialog box is displayed.
  6. Provide the following details:
    • Server:
      dm-virtualpostgres.cloud.rockwellautomation.com
      (Production URL).
    • Port: Provide port number as 5432.
    • Database: The name of the project in FactoryTalk DataMosaix.
    • Authentication: By default, Username and Password is selected.
    • Username: Refer to the Client ID generated while registering the application.
    • Password: Refer to the Client Secret generated while registering the application.
      NOTE:
      SSL is always enabled in both checked and unchecked conditions of the
      Require SSL
      checkbox.
  7. Click
    Sign In
    .
    PostgreSQL Dialog
  8. Drag and drop a table to open campus and click
    Update Now
    to get the table data.
    Update Table Data
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal