- Extractors
- Analyze Data
Modify Capability
If you are a Project Administrator, you can modify the capabilities associated with the capability groups. Follow the instructions:
- In theCapability Group Detailpage, from theCapabilitiessection, choose the capability tile you want to modify and clickView Details.The right pane displays the selected capability’s name, along with the applied actions details.
- Make necessary changes as required.
- ClickApply.NOTE:You need to save the changes in theCapability Group Detailpage in order to apply the changes. If you want to undo any changes, clickRevert.
- ClickSave.
Provide Feedback