Create Project

Create Project

In FactoryTalk DataMosaix a project is the medium through which members can register applications and extractors for performing data analytics and data visualization. The create project feature is governed by role-based access. You can create project if you are an owner or an administrator of an organization in FactoryTalk Hub. Once you create a project, you must add members in the organization. Once the members join the organization, you should assign them roles in FactoryTalk DataMosaix to use the application. The members can register applications and extractors to ingest and visualize data in FactoryTalk DataMosaix.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal