- Extractors
- Analyze Data
Configuring FT Optix to connect to DataMosaix - Continuation
- Restart the FT Optix Studio and open the project.
- If you have installed the connector file in the exact location of your Optix project, an FT DataMosaix Store will be created in the FT Optix DataStore. To view it, navigate to theProject view>DataStoresand click on it to view all the stores created within.FT Optix DataStores
- Select theFTDataMosaixStoreto view the Properties pane.
- In thePropertiespane, provide the following information:
- PushInstance- Provide the instance which needs to be pushed to the Cognite.Push Instance
- ConfigFolderPath- Provide the exact path to the downloaded config.yml file.NOTE:Ensure that the file name 'config.yml' remains unchanged, as altering it may result in failure.
- To run the emulator, in the main toolbar, click Run on Emulator [
].
TheNetLogic security warningdialog box is displayed. - ClickProceed.The project will get saved, and the application will initiate deployment and run the project. The following actions will take place automatically:
- Asset creation.
- Subscribe to tags.
- Creation of flexible data model.
TIP:In the bottom left corner, navigate toEmulator Output>Messagesto view the status of actions with the timestamp details.View Messages
Provide Feedback