- Extractors
- Analyze Data
Run the Optix Project in Optix Panel Runtime
To run the Optix project in the Optix Panel runtime, the user needs to configure the Optix Panel in FT Optix.
Perform the following steps to configure the Optix Panel in FT Optix:
- Click theEmulatordrop-down list and clickLocal.Drop-down Selection
- Click the [+] icon to add new target device.Add New Target Device
- Provide the following details:
- Name: Provide name of the target device.
- IP Address: Provide the IP Address of Optix Panel.
- Username: Provide the username of Optix Panel.
- (Optional) Destination Path: Provide the target device deploying destination path.
- Select theEncrypt project,Transfer source project,Transfer application files, andTransfer optimized projectcheckboxes.
- ClickSelect.FTOptixStudio Window
- Follow the steps from the above section (Configuring FT Optix to Connect to DataMosaix – Continuation).
- Place theconfig.ymlfile in theproject directory > ProjectFilespath.Copy Config File
- Provide the config file path as%PROJECTDIR%.ConfigFolderPath
Provide Feedback