Perform the following steps to view the newly created asset:
FactoryTalk Datamosaix: On the Management Console, click the
Modeling
tab to view the newly created assets.
Model Listing
TIP:
If you see the newly created assets on the Model Listing page, click the Refresh [ ] icon to update the page.
Cognite Data Fusion: Navigate to
Data Explorer
>
Assets
.
Assets
When you run the connector, you will see the Flexible Data Models
NOTE:
When the user runs the connector using the extractor config file, the extraction pipeline is updated with the associated dataset to track the extractor's run history and the current status of the pipeline.