Edit Role

Edit Role

If you are a project administrator, you can modify the assignment of roles. You can either assign a role or remove an existing role for a member.
Perform the following steps to edit the roles:
  1. On the Management Console, select the
    Manage Access
    tab.
  2. In the
    Actions
    column, click the [] icon next to the member.
    Member Listing
    NOTE:
    • If no roles are assigned, the [+] icon is enabled
    • If all roles are assigned, the [+] icon is disabled.
    • If there are some roles unassigned, then both, [+] and [] icons are enabled.
    The
    Edit all Roles
    page is displayed, and it displays the assigned and unassigned roles.
    NOTE:
    Click the [] icon to expand the role and view its capabilities. Click the icon again to collapse it.
    Role Capabilities
  3. Select or clear the checkbox adjacent to a role to assign or remove the role.
    NOTE: The user can use the search bar to find a specific role.
  4. After you make all the changes, click
    Apply
    .
    The "
    Roles updated
    " message is displayed.
    Edit Roles
    The
    Member Listing
    page displays the modified roles in the
    Roles
    column.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal