FactoryTalk DataMosaix Member Roles

FactoryTalk DataMosaix Member Roles

FactoryTalk DataMosaix has seven predefined roles. Each role has a separate set of capabilities and privileges. Based on the task a member wants to perform, they are assigned roles. A project admin can change roles of other members.
The following table provides information about a role and the tasks that you can perform with that role:
FactoryTalk DataMosaix Role-Functionality Matrix
If you are
You can
Project Admin
  • Create Projects
  • View Members and roles
  • Assign roles
  • Unassign roles
  • Delete members
  • View Extractors
  • View Applications
Data Configurator
  • Register Extractors
  • View Extractors
  • Edit Extractors
    • Regenerate client secret
  • Delete Extractors
  • View Applications
Data Scientist
  • Register Applications
  • View Applications
  • Edit Applications
    • Regenerate client secret
  • Delete Applications
  • View Extractors
  • Create Assets
  • Update Assets
  • View Assets
  • Delete Assets
Application User
  • View Applications
  • View Extractors
Application Developer
  • View Applications
  • View Extractors
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal