View messages
View error, warning, and information messages for the logic in your ladder diagram in the project. The
Messages
tab allows you to go to the location associated with the message and correct the issue. The ladder diagram does not have to be open to review messages. - If theOutputpane does not appear, in the pane bar, selectOutputor selectView > Output > Messages.
- InOutputunderMessages, select the option to view the desired messages:
- Entire project. View messages for the entire project. This is the default.
- Current tab. View messages for the current tab in focus.
- InDescription, read the description of the message.
- InLocation, select the link to open the location in the ladder diagram so that you can resolve the issue.TIP: To sort by location, select theLocationcolumn header to toggle between ascending and descending order.
- (optional) InSearch, type a portion of the description or message.Messagesreturns rows that meet the search criteria.
Provide Feedback