- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- NetLogic
- Tutorials
- Dynamic links tutorial
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
Create variables
Use C# APIs to create variables in the
FactoryTalk Optix Studio
project and return the corresponding C# objects.The APIs are supplied by the
InformationModel
class, displayed by the FTOptix.HMIProject
module.Provide Feedback