Add Project to Source Control
Use this dialog to add a project to source control.
Parameter | Description |
---|---|
Selected folder | Displays the currently selected folder within source control view. |
Look in | Select the directory in the AssetCentre archive where the project to open or import resides. (The last open location is remembered upon subsequent returns.) |
Up One Level - ![]() | Move up one level in the directory tree. Active when logged in to a server or database and not at the top level of the tree. |
View Menu - ![]() | Select the view type (view list of file names or list of file names with the username). Active when logged in to a server or database. |
Login - ![]() | Log in to a specific server and attach to a specific database. |
Select this button to Manage Server Registrations - ![]() | Open dialog to manage one or more servers or database combinations. |
Select Version or Label for the Operation - ![]() | Select an archived element based off of either version or a label. Active when file selected. |
Search for Files or Folder - ![]() | Search for either files or folders within the current archive database. Active when logged in to a server or database. |
Help - ![]() | Display help about using source control. |
New Folder | Create a new folder within the source control database. Select New Folde r to open the New Folder dialog. |
Comments | Enter a comment up to 255 characters in length. Comments longer than 255 characters are truncated. |
Check out after adding to source control | If checked, the file is checked out immediately after it is added to source control. If not checked, the file is reopened as a file copy. This control is checked by default. |
OK | Add the open project to the selected folder. A prompt to save appears if unsaved edits. |
Select this button to Cancel | Close the dialog and return to the open project without adding the project to source control. |
Help | View help about dialog. |
Provide Feedback