Generate instruction signature
Generating a signature will seal instruction and prevent modifications. Generate instruction signature?
- Clicking Yes generates a signature, and the Add-On Instruction becomes sealed (modifications are prevented).
- Clicking No does not generate a signature, and the Add-On Instruction remains unsealed (modifications are allowed).
Provide Feedback