Tip of the Day Dialog Box Overview

Tip of the Day Dialog Box Overview

Receive helpful information on using the
Logix Designer
application from this dialog box.
This dialog box has the following parameters:
Parameter
Description
Tip
A message that provides you with helpful information on using the
Logix Designer
application.
Show Tips on Startup
Check this box if you want a new tip to appear each time you start the
Logix Designer
application.
Next Tip
Click this button to go to the next tip.
Close
Click this button to close the Tip of the Day dialog box.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal