Change Equipment Sequence Editor preferences dialog box

Use the
Change
Equipment Sequence
Editor preferences
dialog box to set preferences for the
Equipment Sequence
editor.
TIP: To open the Workstation Options - Change Equipment Sequence Editor preferences dialog:
  1. Select
    Tools > Options
    .
  2. On the
    Workstation Options
    dialog box, select
    Equipment Sequence Editor
    .
Select or clear the check boxes for the following settings.
  • Auto-Scroll During Online Monitoring
    When you monitor an
    Equipment Sequence
    , the Monitor window auto-scrolls so that the active sequence step is always in the window.
  • Show Cross Reference Grid (selected by default)
    The background of the
    Equipment Sequence
    Editor identifies columns with letters and rows with numbers and displays a grid to identify positions of sequence elements.
  • Show Sheet Boundaries (selected by default)
    The background of the
    Equipment Sequence
    Editor indicates page boundaries based on the configured paper size.
Select
OK
to apply the settings.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.