Change modes effect on sequence and step commands
Use the change mode to toggle an
Equipment Sequence
between Automatic
and Manual
mode.Mode effect on sequence commands
The following table shows the mode effect on sequence commands.
Command | Automatic Mode | Manual Mode |
Start, Hold, Stop, Abort, Restart, Reset | Allowed | Ignored |
Pause, Auto Pause, Resume | Allowed | Ignored |
Clear Failures on a sequence | Allowed | Allowed |
Force Transition Expression to Evaluate TRUE | Not allowed | Allowed |
Change Active Step | Ignored | Allowed |
Mode effects on step commands
Commanding a step is the same as commanding the Equipment Phase, except it is done through the sequence. The following table shows the mode effect on step commands.
Command | Automatic Mode | Manual Mode |
Start, Hold, Stop, Abort, Restart, Reset | Ignored | Allowed |
Pause, Auto Pause, Resume | Ignored | Allowed |
Clear Failures on a sequence | Ignored | Allowed |
Force Transition Expression to Evaluate TRUE | Not allowed | Allowed |
Provide Feedback