- Studio 5000 Logix Designer
- Tasks, programs, and routines
- Add-On Instructions
- Controller Organizer
- Logical Organizer
- Alarms
- Tag-based alarms
- Tag Editor and Data Monitor
- Configure settings for Tag Editor and Data Monitor
- Equipment phases
- Equipment Sequences
- Equipment Sequence Diagrams
- Ladder Editor
- Structured Text Editor
- Sequential Function Chart Editor
- Define the steps of an SFC process
- PlantPAx instruction properties
- Controller Properties
- Editing Controller Properties
- Controller Security
- Source Protection
- License Source Protection for Routines and Add-On Instructions
- Module Information
- 1756 ControlLogix I/O Modules
- Instruction Set
Error - Failed to import component
The component (Program, Phase, or Add-on instruction) could not be imported. This error can occur for the following reasons.
Import target is no longer valid
This error occurs when Online in Remote Run Mode if an Import command cannot be completed because the import target is no longer valid. The specified component is discarded upon import.
Locked component is from a different controller family
A locked component from a different controller family cannot be imported while online. The component must be recompiled to support the current controller and then re-locked.
Provide Feedback