Renaming a Connector Group

Renaming a Connector Group

Wire connectors that share the same connector name in a function block can be changed using the
Rename Connector Group
command.
If there are wire connector(s) with the new name, the renamed wire connectors merge with the existing connectors.
To rename a connector group:
  1. Right-click a connector and then click
    Rename Connector Group
    .
  2. Type or select the new name and press
    Enter
    .
    All instances in the group are changed to the new name.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal