Error importing changes

The import was canceled due to errors. No changes have been made to the project. Check the contents of the output window to determine why the import failed.
This error can occur for these reasons:
License Source Protection is not supported on this controller
One or more components in the project are protected by License Source Protection, which is not supported on this controller in this version of the
Logix Designer
application. If possible, remove License Source Protection from the project or components before importing them.
Imported project protected by a different security authority
The project to be imported is protected by a different primary security authority than the current project. Imported content must be protected by the same primary security authority as the current project.
Data was corrupted
The imported project data might be corrupted.
Project contains unsupported components
The imported project contains components that are not supported by the current controller type or the current version of the
Logix Designer
application.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.