- Studio 5000 Logix Designer
- Tasks, programs, and routines
- Add-On Instructions
- Controller Organizer
- Logical Organizer
- Alarms
- Tag-based alarms
- Tag Editor and Data Monitor
- Configure settings for Tag Editor and Data Monitor
- Equipment phases
- Equipment Sequences
- Equipment Sequence Diagrams
- Ladder Editor
- Structured Text Editor
- Sequential Function Chart Editor
- Define the steps of an SFC process
- PlantPAx instruction properties
- Controller Properties
- Editing Controller Properties
- Controller Security
- Source Protection
- License Source Protection for Routines and Add-On Instructions
- Module Information
- 1756 ControlLogix I/O Modules
- Instruction Set
Rename a routine
You can rename a routine using the
Routine Properties
dialog box.To access the
Routine Properties
dialog box, right click the routine whose properties you want to change from the Controller Organizer
or Logical Organizer
, and choose Properties
. The Routine Properties
dialog box appears, with the General
tab selected.
TIP:
You cannot change the name for Add-On-Instruction routines or equipment phase state routines.
To rename a routine:
- InName, enter the appropriate name for the routine.
- InDescription, enter a description of the routine.
Provide Feedback