PVLVMP time settings
Use the
Advanced > Time configuration
tab on the PVLVMP Properties dialog box to configure time parameters for Process Mix Proof Valve (PVLVMP) instructions.To configure time settings for PVLVMP instructions
- On the instruction in the routine, perform one of these actions:
- On the Ladder or FBD instruction, select
.
- In the Structured Text editor, right-click the tag name and selectConfigure <tag name>.
- Select theAdvanced > Time configurationtab.
- Configure these settings:
- Time to sound audible on commanded energize. Enter the number of seconds to sound an audible notification when the valve is commanded to move from the closed position.
- Time after valve command for feedback before fault. Enter the number of seconds to allow for valve state feedback after a command. If feedback is not received within the allotted time, the instruction reports aFailurestatus.
- Time to close seat when pulsing seat for cleaning. Enter the number of seconds to close the seat when pulsing for cleaning.
- Time to lift seat when pulsing for cleaning.Enter the number of seconds to lift the seat when pulsing for cleaning.
- SelectApply.
Provide Feedback