PAIM process variable values
Use the
General
tab on the PAIM Properties
dialog box to monitor values for the process variable (PV) inputs for Process Multi Sensor Analog Input (PAIM) instructions.To monitor process variable values for PAIM instructions
- On the instruction in the routine, perform one of these actions:
- On the Ladder or FBD instruction, select
.
- In the Structured Text editor, right-click the tag name and selectConfigure <tag name>.
- When online with the controller, monitor theDevice stateandDevice issuesindicators at the bottom left of the dialog box:
- Device state. Displays the current device status: PV good, PV uncertain, or PV bad.
- Device issues. Displays fault conditions: None, Any reject, Min good, Fail, or Configuration error.
- Monitor the input values for the process variable and signals.TIP: Use theAdvancedtab to add labels for the inputs. Use theHMItab to add a label that identifies the units for the inputs.
Provide Feedback