Using a common control platform across your entire installed base of variable frequency drives lowers integration, operation and maintenance costs. That’s why the new PowerFlex 6000T medium voltage drive shares the same powerful control hardware and firmware as PowerFlex 755T low voltage drives. The PowerFlex 6000T also has an Add-On Profile in the Studio 5000 design environment. The Add-On Profile is the preconfigured data translator, visual user interface and data configurator all rolled into one. It is also the primary tool that sends drive data to the common control system.
Click to download image.
In addition to simplified operation and integration, the PowerFlex 6000T has other new features that make it easier to use including a larger 10” color touchscreen enhanced HIM, Forensic Data Recorder functionality for faster troubleshooting, extensive input power monitoring capabilities for kW, kVA, kVAR, elapsed kWh, MWh, power factor, and quick and secure flash-over-fiber firmware updates for all main control boards and power cells from a single file.
PowerFlex and Studio 5000 are trademarks of Rockwell Automation Inc.
Published April 2, 2020