Tag Editor validation errors
The
Tag Editor
grid displays validation messages. Messages that have a tag validation error that needs to be addressed are preceded by an error icon:
Mouse over the icon for details or view the error in the
Messages
tab of the Output
pane.
Scenario | Error | Example |
---|---|---|
Enter an invalid value of any of the cells of Tag Editor grid. |
| |
Select an array tag with more than 3 dimensions. | The array has too many dimensions. Enter 3 or fewer array dimensions. | TAG001[2,2,2,2] |
Select an array tag with dimensions when the value of the dimension is out of the range. | The array dimensions are out of range. Enter a value between 1 and 65535. | INT TAG001[2,2,9999999999999999999999999] |
Manually enter an unsupported or nonexistent datatype. | Unable to resolve the reference to the [datatype]. | TAG001___________________ |
End a tag name with multiple underscores. | Cannot contain consecutive underscores. | |
End a tag name with an underscore. | [Tag name] must end with a character other than underscore. | TAG001_ |
Enter a syntax error on a datatype or tag name. | Syntax Error: The element contains a syntax problem. Select OK to modify the element. | %TAG001 |
Enter a name that contains characters that are not alphanumeric or an underscore. | [Tag name] can only contain alphanumeric characters and underscore. | 56TAG001 |
Enter an existing tag name. | [Tag name] already exists |
:
Provide Feedback