Create project variables
Create the Speed and Acceleration variables to use them in the UI design.
- InProject view, create two variables by right-clicking theModelfolder, and selecting .
- Rename the variables by hovering-over each variable, selecting, and entering:
- Speed
- Acceleration
Provide Feedback