Set up FactoryTalk Optix Runtime Tools on Ubuntu 22.04 devices
NOTE:
FactoryTalk Optix Runtime Tools currently supports Ubuntu 22, x64 CPUs.
The FactoryTalk Optix Runtime Tools for Ubuntu 22.04 consists of the FactoryTalk Optix Application Update Service and the FactoryTalk Optix Entitlement Command Line Interface (CLI).
- Install and update Ubuntu desktop 22.04.
- Enter the following commands:
- sudo apt-get update
- sudo apt-get upgrade
- sudo apt-get install libxcb-cursor0
- cd ~/Downloads
- tar xvf FactoryTalkOptixRuntimeToolsSetup_Ubuntu_22_x64_[version].Beta.tar.gzThis installation package includes two files:
- TheFTOptixApplicationUpdateService.Ubuntu_22_x64.[version].shfile, to install the Update Service.
- TheFTOptixEntitlementCli.Ubuntu_22_x64.[version].shfile, to install the Entitlement Manager.NOTE: See Activate a Runtime entitlement on Ubuntu 22.04 devices to learn more about the entitlement activation procedure.
- chmod +x FTOptixApplicationUpdateService.Ubuntu_22_x64.[version].sh
- sudo ./FTOptixApplicationUpdateService.Ubuntu_22_x64.[version].shIMPORTANT:
- If you use a Rockwell Automation driver, entersudo apt-get install libglib2.0-bin
- If you use an Open DataBase Connectivity (ODBC) driver, entersudo apt-get install libltdl7
- If you use native presentation engine in your FactoryTalk Optix Applications, entersudo apt-get install libevent-dev
TIP: To run the script in silent mode, add the-sflag:./FTOptixApplicationUpdateService.Ubuntu_22_x64.[version].sh -s. Silent mode is useful if you do not want to interact with the script and for various automations.
- Restart Ubuntu and proceed with the entitlement activation.
NOTE:
If the project includes a videoplayer, install additional packages by using the
sudo apt-get install gstreamer1.0-libav ubuntu-restricted-extras
command.Provide Feedback