FactoryTalk Optix Studio setup overview

Once you have download
FactoryTalk Optix Studio
from the FactoryTalk Hub and installed it, you can start using it without purchasing an entitlement.
  1. Access the FactoryTalk Optix landing page. See FactoryTalk Optix landing page.
  2. Authenticate as required.
  3. On the FactoryTalk Optix landing page, select
    Download
    .
    NOTE: See FactoryTalk Optix landing page for further details on this subject.
  4. Select the checkbox next to
    FactoryTalk Optix Studio
    and in the upper right corner, select the first instance of
    Download Now
    at the top.
  5. Scroll to read the EULA and select
    Accept and Download
    .
    The download progress is displayed in the
    Download Manager
    .
  6. When the download is complete, in the lower left corner, select the up arrow to select
    Show in  folder
    and then double-click the execution file.
  7. Select
    I accept the agreement
    and complete the setup to install FactoryTalk Optix Studio.
FactoryTalk Optix Studio is installed and ready to use.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.