Select a client device
Select an already configured target client device to deploy
FactoryTalk Optix Applications
over the network to the client device.- From the main toolbar, next to, select the target client device drop-down.Run
- (optional) InClient device settings, to display only the active remote client devices, toggle
.
TIP: Refresh remote client devices by selecting.
- Select a client device.
- ClickSelect.
Provide Feedback